Drag to rotate
sku: OAK-D-SR-PoE
OAK ToF
US $479
Hardware update
Indoor and controlled lighting
OAK Time of Flight is a camera that emphasizes improved short-range accuracy when compared to the standard OAK-D and further expands our catalog of robotic vision solutions. It employs Time of Flight (ToF) VGA sensor, which enables accurate measurement of the depth of objects in a scene, resulting in more precise focusing and improved low-light performance.
Key Features
- IR dot projector
- Time of Flight (ToF) VGA (640x480 @ 30fps)
- Two OV9782 (1 MP Color Global Shutter)
- IP67 rated enclosure (please see technical specifications below)
- M12 X-coded connector
- M8 IO connector
- PoE circuitry