OAK-D Pro
Available on backorder. New batch in late June 2022.
The OAK-D Pro is an upgraded version of OAK-D, featuring an IR laser dot projector (active stereo) and IR illumination LED (for “night vision”). It’s also smaller and lighter than the OAK-D.
Available in two variants:
Both the Fixed-Focus and Auto-Focus variants have fixed-focus grayscale stereo cameras. The Auto-Focus vs. Fixed-Focus variants of OAK-D-Lite differ only in the 12.3 MP color camera. Fixed-Focus has the lens fixed in place mechanically and cannot move, whereas Auto-Focus has an electromagnet that controls the lens position dynamically.
- Auto-Focus can focus on objects dynamically, which is mainly useful for objects within 50cm of the device
- Fixed-Focus is recommended for heavy-vibration applications (e.g., drones, lawnmowers, bikes w/out suspension, etc. (see video)
Both Auto-Focus and Fixed-Focus can clearly see objects beyond 50 cm, working between 50 cm and infinity. Auto-Focus has the advantage that it can focus on objects as close as 10cm (see video).
Features:
-
Active Laser Depth: depth with no ambient light
-
Active Blanket IR illumination: computer vision with no ambient light
-
4 TOPS of processing power (1.4 TOPS for AI)
-
Run any AI model, even custom architectured/built ones
-
Encoding: H.264, H.265, MJPEG - 4K/30FPS, 1080P/60FPS
-
Computer vision: warp/dewarp, resize, crop, edge detection, feature tracking
-
Stereo depth perception at 120 FPS with filtering
-
Object tracking: 2D and 3D tracking
-
Dimension: 97x29.5x22.9 mm
- Weight: 91g
Camera Specifications:
Color camera |
Stereo pair |
|
Sensor |
IMX378 |
OV9282 |
DFOV / HFOV / VFOV |
81° / 69° / 55° |
81° / 72° / 49° |
Resolution |
12MP (4032x3040) |
1MP (1280x800) |
Focus |
Auto-Focus: 8cm - ∞ |
Fixed-Focus: 19.6cm - ∞ |
Max Framerate |
60 FPS |
120 FPS |
F-number |
2.0 |
2.2 |
Lens size |
1/2.3 inch |
1/4 inch |
For more information please check the Documentation and Github repository.
Laser dot projector projects many small dots in front of the device, which helps with disparity matching, especially for low-visual-interest surfaces (blank surfaces with little to no texture), such as a wall or floor. The technique that we use is called ASV - conventional active stereo vision - as stereo matching is performed on the device the same way as on OAK-D (passive stereo).
Blanket IR LED illumination allows perceiving low-light and no-light environments. You can run your AI/CV processes on frames that are illuminated by the IR LED. Note that the color camera doesn’t perceive IR light, so you would need to use a mono camera stream for your AI/CV processes.
Includes:
- OAK-D-Pro camera
- Y-Adapter
- USB-C cable
Reference Numbers:
PN: OAK-D-Pro Auto-Focus
MN: A00546
PN: OAK-D-Pro Fixed-Focus
MN: A00565
Shipping
Returns
Help
Resources
Shipping cost is based on location and calculated on checkout. We provide multiple shipping carriers services.
We ship from Hong Kong. Import taxes and fees may apply.
We want you to be 100% satisfied with your purchase. Items can be returned or exchanged within 60 days of delivery. Please contact us at support@luxonis.com for details.
For help, please contact us at support@luxonis.com
For more information, please go to Hardware Documentation, DepthAI Documentation and GitHub Repository. You can also join us on Discord.