- Description
- Package Includes
Description
For more information about frame synchronization please follow link to the documentation.
FSync Y adapter provides true hardware frame sync capability precisely syncing frames on multiple cameras. 2x female-to-male cables need to be used with the FSync Y-adapter:
- cable connecting the Y-adapter to the OAK's M8 connector
- cable connecting to the next Y-adapter in the chain, so it can be daisy-chained
One can daisy-chain multiple OAK cameras as per wiring schematics below. Multiple cameras can be daisy-chained.
Specifications
- Dimension: 23.5x33x10 mm
- Weight: 5g
Package Includes
Package contains:
- 1x FSYNC Y-adapter
- 2x M8 2 meter cable (male to female)