Check out our new store Check out our new store

$299.00 VAT incl.

In stock
24 PCS
OAK-1 Lite Camera

Note! This product is for development purposes and has to be hand calibrated. Please see the documentation for more information.

For more details about the device please see the technical details below.

If you are looking for a factory-calibrated device, please see OAK-D-Pro W.

Read more

SKU: A00506N/A
Out of stock

Description

  • The optics on these early development models have no filtering and are "wide open" in terms of spectral response - meaning they let in all visible light and all IR light.
  • Production versions will have a filter that lets in visible light, and a narrow notch around the IR laser dot projector and IR LED wavelength, both of which are 940nm.
  • So this version will (a) appear to have "dim" IR laser and IR LED illumination - as these absorb much ambient IR, which will overwhelm the IR laser and LED and (b) will have inferior optical performance as a result of the ultra-wide spectral input into the image sensor. The final production version will address both of these with the filtering described in `2` above.
  • Nonetheless, these optics give an idea of the field of view, depth, etc. It is simply likely that the IR illumination, active stereo depth, and passive depth will all perform better in the final production version in the presence of the filtering described in `2`.
Camera Specifications
Specification Central RGB Camera Stereo Pair Cameras
Sensor OV9782 OV9282
DFOV / HFOV / VFOV 150° / 127° / 79.5° 150° / 127° / 79.5°
Resolution 1MP (1280x800) 1MP (1280x800)
Focus FF: 19.6 cm - ∞ FF: 19.6 cm - ∞
Spectral Range Full Full
Max Framerate 60 FPS 120 FPS
  • OAK-D Pro W Dev camera
  • Dot projector

Safety Icon

This product is classified as a Class 1 Laser Product under the EN/IEC 60825-1, Edition 3 (2014) internationally.

Sunday,Monday,Tuesday,Wednesday,Thursday,Friday,Saturday
January,February,March,April,May,June,July,August,September,October,November,December
Not enough items available. Only [max] left.
Shopping cart

Your cart is empty.

Return To Shop

OAK-D Pro W Dev

$299.00