OAK-D Pro W Dev
Available for preorder. Limited stock in late June 2022.
More information and progress here. Setup documentation here.
Important technical note:
- The optics on these early development models have no filtering and are "wide open" in terms of spectral response - meaning they let in all visible light and all IR light.
- Production versions will have a filter that lets in visible light and a narrow notch around the IR laser dot projector and IR LED wavelength, both of which are 940nm.
- So this version will (a) appear to have "dim" IR laser and IR LED illumination - as these absorb much ambient IR which will overwhelm the IR laser and LED and (b) will have inferior optical performance as a result of the ultra-wide spectral input into the image sensor. The final production version will address both of these with the filtering described in `2` above.
- Nonetheless, these optics give an idea of field of view, depth, etc. It is simply likely that the IR illumination, active stereo depth, and passive depth will all perform better in the final production version in the presence of the filtering described in `2`.
Note! This product might be not calibrated or hand calibrated, resulting in a less accurate depth map.
Includes:
- OAK-D Pro W Dev camera
Reference Numbers:
PN: OAK-D-Pro-W-Dev
MN: A00506
Shipping
Returns
Help
Resources
Shipping cost is based on location and calculated on checkout. We provide multiple shipping carriers services.
We ship from Hong Kong. Import taxes and fees may apply.
We want you to be 100% satisfied with your purchase. Items can be returned or exchanged within 60 days of delivery. Please contact us at support@luxonis.com for details.
For help, please contact us at support@luxonis.com
For more information, please go to Hardware Documentation, DepthAI Documentation and GitHub Repository. You can also join us on Discord.